Analog Value Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.

Table 1. Analog Value Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Flags 1

BACnet Flags1

Initial Value

Values/Options/Range

COV Increment 2

Real Value

CW

BW

0.01

Any value > 0

Display Precision

One value from a set

CW

CW

10ths

 

Max Value

Real value

CW

BW

1.7E38

This value is not writable for FEC objects.

This value is writable if the AV is the ZN-SP on a Net Sensor. This method is the only way to set the range for the Net Sensor.

Min Value

Real value

CW

BW

-1.7E38

This value is not writable for FEC objects.

This value is writable if the AV is the ZN-SP on a Net Sensor. This method is the only way to set the range for the Net Sensor.

Out of Service

True or False

 

W

False

Always False

Present Value

Real value

DRW

DRW

   

Priority Array

Set of values

       

Reliability

One value from a set

W

BW

Reliable

See the attribute description for details on Reliability.

No Fault Detected (Reliable), Over Range, Under Range, Unreliable Other

Status Flags

Series of True or False values

 

B

False,

False,

False,

False

See the attribute description for details on Status Flags.

In Alarm, Fault, Overridden, Out of Service

Units

One type from a set

W

W

Blank

 
1 B - Exposed as Standard BACnet Property, C - Configurable, D - Default Attribute for Display, R - Affected by Object Reliability, W - Writable
2 This attribute is required if the object supports COV reporting.