Analog Value Object - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Analog Value (AV) objects have similar software characteristics and capabilities to Analog Input Objects; however, Analog Value objects are not associated with any physical hardware and are the result of a control process or operator entry. This object allows you to hold an analog value for other objects to reference. For example, an Interlock Object can reference and base its operation on an analog value such as Outdoor Air Temperature Low Limit.

For general information on BCPro objects, see Common Object Attributes.