Reliability - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English
Examples:
  • Reliable - No detectable faults
  • Unreliable High - Present Value is greater than the Max Value
  • Unreliable Low - Present Value is less than the Min Value.

When Out of Service is True, the Reliability attribute may be written directly.

Back to Analog Output Attributes.