Analog Output Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.

Table 1. Analog Output Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Notes 1

BACnet Notes1

Initial Value

Values/Options/Range

COV Increment

Real value

CW 2

BW

0.1

Any value > 0

Device Type

Text

CW

W

Null

Limit: 20 characters

Display Precision

One value from a list

CW

CW

10ths

 

Max Value

Real value

CW

BW

100.0

This attribute is not Writable for a PAO.

Min Value

Real value

CW

BW

0.0

This attribute is not Writable for a PAO.

Out of Service

True or False

CW

BW

   

Present Value

Real value

DNRW

BW

0.0

 

Priority Array

Set of values

       

Reliability

One value from a set

W

BW

0

No Fault Detected (Reliable), Open Loop, Shorted Loop, No Output, Unreliable Other

Resolution

Real value

 

B

0.1

 

Status Flag

Series of True or False states

 

B

False,

False,

False,

False

In Alarm, Fault, Overridden, Out of Service

Units

One value from a list

CW

W

%

This attribute is not Writable for a PAO.

Use COV Min Send Time

True or False

W

 

False

 
1 B - Exposed as Standard BACnet Property, C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Object Reliability, W - Writable
2 For MS/TP Analog Outputs, COV Increment may not be writable, based on its configuration.