Analog Output Object - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English
The AO object’s attributes represent the external, visible characteristics of an analog output. This object integrates BACnet controllers into supervisory controllers, resulting in:
  • a consistent interface to point objects for all controller types, so they appear as a homogenous set to the user interface
  • flexibility in point mapping
  • permanent update of setpoints in controllers. The user has the ability to write to the permanent memory of some controllers.
  • support for all BCPro controllers
  • For example, this object allows you to command a damper to a given position from a supervisory controller.

For general information on BCPro system objects, see Common Object Attributes.