Use COV Min Send Time - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Configures the MS/TP Analog Input object to send COV messages on a periodic basis instead of on every change of value that exceeds the COV Increment . This attribute is typically set to True for objects with values that fluctuate greatly, such as air pressure, to decrease the number of COV messages. The change of value still must exceed the COV Increment to be reported. This attribute is available only on BCPro system field devices, such as the MS/TP field devices.

Back to Analog Input Attributes.