Reliability - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Indicates whether the Present Value is unreliable.

Examples:

  • Reliable - No detectable faults
  • Unreliable High - Present Value is greater than the Max Value.
  • Unreliable Low - Present Value is less than the Min Value.

When Out of Service is True, the Reliability attribute may be written directly.

Back to Analog Input Attributes.