Analog Input Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.
Table 1. Analog Input Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Notes 1

BACnet Notes1

Initial Value

Values/Options/Range

COV Increment

Real value

CW 2

BW

0.1

Any value > 0

Device Type

Text

CNW

CNW

Null

20 Character Limit

Display Precision

One from a set

CW

CW

10ths

 
Max Value

Real value

CW

BW

1.7E38

 
Min Value

Real value

CW

BW

-1.7E38

 
Out of Service

True or False

CW

BW

False

 
Present Value

Real value

DNRW

DNRW

   
Reliability

One state from a set

W

BW

Reliable

No Fault Detected (Reliable), No Sensor, Over Range, Under Range, Open Loop, Shorted Loop, Unreliable Other

Resolution

Real value

 

B

   
Status Flags

Series of True or False states

 

B

False,

False,

False,

False

In Alarm, Fault, Overridden, Out of Service

Units

One value from a list

CW

W

Deg F

 
Update Interval

Number

 

B

0

0–65,535

Units = hundredths of a second

Use COV Min Send Time

True or False

W

 

False

Applies to MS/TP Analog Inputs.

1 B - Exposed as Standard BACnet Property, C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Object Reliability, W - Writable
2 For MS/TP Analog Inputs, COV Increment may not be writable, based on its configuration.