Analog Input Object - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

The AI object processes data from a physical analog input point that resides on a field device and presents the data to the BCPro user interface in a consistent format that is independent of the source. Analog Input Objects appear under the field device object in the All Items navigation tree.

When the source of the data is an analog input in an integrated BACnet device, the Analog Input Object exchanges data with the native analog object in the source to synchronize attribute data that are common to both. The source is identified under the hardware tab of the Analog Input Object.

For general information on BCPro system objects, see Common Object Attributes.