ActionQ Operation - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

About this task

The ActionQ shows the status of commands and allows you to monitor, enable or disable, delete, and reschedule commands. See the ActionQ Interface section. The ActionQ receives a command from a wizard and executes the command based on the date, time, and other specified parameters.

The order of operation is as follows:

Procedure

  1. The ActionQ receives a command from the Manage Archive Wizard wizard.
  2. The ActionQ initiates the command (for example, starts the upload process)
  3. The ActionQ interface displays the progress and final status of the command.

Results

Note: The final status remains on the ActionQ screen until you delete it or it is automatically deleted after a user-defined number of days (1–30).
Note: At this time, the ActionQ only supports upload, download, upgrade device, and synchronization commands from the Manage Archive Wizard. See the Upload, Download, Synchronize, and Upgrading Device sections.