The ActionQ contains three main screens.
|
Screen |
Description |
|---|---|
|
ActionQ |
Allows you to view active, scheduled, and completed commands. This screen is the main screen of the ActionQ interface and has three tabs:
Note: A command is pending when it has not been issued because the recipient device is busy as a result of too many incoming commands.
Note: Once a command is issued, it may be complete before a command to disable, delete, or reschedule reaches it.
|
|
ActionQ Reschedule a Command Dialog Box |
Note: If you schedule multiple commands to occur at the same time, not all commands may begin at the specified time because they are waiting for other commands to complete.
|
|
ActionQ View Status Dialog Box |
|