Dynamically Creatable: No
Dynamically Deletable: No
Property Name |
Required |
Optional |
Proprietary |
Property ID |
Data Type |
Writable |
Range |
---|---|---|---|---|---|---|---|
OBJECT_NAME |
X |
77 |
|||||
OUT_OF_SERVICE |
X |
81 |
|||||
PRESENT_VALUE |
X |
85 |
X |
||||
INACTIVE_TEXT |
X |
46 |
X |
40 characters max |
|||
ACTIVE_TEXT |
X |
4 |
X |
40 characters max |
|||
COS_TIME |
X 1 |
16 |
|||||
COS_COUNT |
X1 |
15 |
X |
||||
STATE_COUNT_RESET |
X1 |
115 |
|||||
ELAPSED_ACTIVE_TIME |
X1 |
33 |
X |
0–4,294,967,295 |
|||
ACTIVE_TIME_ RESET |
X1 |
114 |
|||||
MIN_OFF_TIME |
X1 |
66 |
X |
0–604,800 |
|||
MIN_ON_TIME |
X1 |
67 |
X |
0–604,800 |
|||
PRIORITY_ARRAY |
X1 |
87 |
|||||
RELINQUISH_DEFAULT |
X1 |
104 |
X |
||||
DESCRIPTION |
X |
28 |
X |
40 characters max |
|||
RELIABILITY |
X |
103 |
X2 |
||||
ACKED_TRANSITIONS |
X 3 |
0 |
|||||
EVENT_ENABLE |
X3 |
35 |
X |
||||
EVENT_TIME_STAMPS |
X3 |
130 |
|||||
EVENT_MESSAGE_TEXTS |
X3 |
351 |
|||||
EVENT_MESSAGE_TEXTS_CONFIG |
X3 |
352 |
X |
||||
EVENT_DETECTION_ENABLE |
X3 |
353 | |||||
NOTIFICATION_CLASS |
X3 |
17 |
X |
1–4,194,302 |
|||
ALARM_VALUE |
X3 |
7 |
X |
||||
NOTIFY_TYPE |
X3 |
72 |
X |
||||
TIME_DELAY |
X3 |
113 |
X |
0–65,535 |
|||
ALARM_STATE |
X |
1006 |
Enumerated |
||||
INTRINSIC_ALARMING_DEFINED |
X |
569 |
Boolean |
X |
|||
ENABLED |
X |
673 |
Boolean |
X |
|||
EXECUTION_PRIORITY |
X |
2197 |
Enumerated |
X |
0–3 |
||
ITEM_REFERENCE |
X |
32527 |
Character String |
||||
OBJECT_CATEGORY |
X |
908 |
Enumerated |
X |
0–249 |
||
ATTRIBUTE_ID |
X |
3365 |
Enumerated |
||||
COMMAND_SIGNATURE |
X |
3366 | Unsigned | ||||
DEFAULT_ATTRIBUTE_VALUE |
X |
3633 |
Boolean |
||||
LAST_RELIABLE_CMD_SIG |
|||||||
PEER_REFERENCE |
X |
748 | Complex |
X |
|||
DIRECTION |
X |
746 |
Enumerated |
||||
ERROR_STATUS |
X |
576 |
Enumerated |
||||
FAILSOFT |
X |
2567 |
Boolean |
X |
|||
IN_TEST |
X |
3368 |
Boolean |
||||
CURRENT_CMD_SIG |
X |
3378 | Unsigned | ||||
CURRENT_RELIABILITY |
X |
3377 |
Enumerated |
||||
STANDARD_NAME |
X |
3670 |
Enumerated |
||||
BACNET_EXPOSED |
X |
3807 |
Boolean |
X |
|||
LAST_RELIABLE_VALUE |
X |
3369 |
Boolean |
||||
DEFAULT_VALUE |
X |
3113 |
Boolean |
X |
|||
TEST_VAL |
X |
3371 |
Boolean |
||||
INPUT |
X |
513 |
Boolean |
||||
OUTPUT |
X |
663 |
Boolean |
||||
CURRENT_VALUE |
X |
3376 |
Boolean |
||||
OFFLINE |
X |
913 |
Boolean |
||||
RESTORE_COMMAND_PRIORITY |
X |
721 |
Bit String |
X |
|||
STATUS |
X |
512 |
Enumerated |
||||
STATES_TEXT |
X |
931 |
Enumerated |
||||
USER_NAME |
X |
2390 |
Character String |
||||
GRAPHIC |
X3 |
32581 |
Character String |
X |
|||
GRAPHIC_ALIAS |
X3 |
32623 |
Character String |
X |
|||
ALARM_MESSAGE_TEXT |
X3 |
536 |
Character String |
X |
255 characters max |