Dynamically Creatable: No
Dynamically Deletable: No
Property Name |
Required |
Optional |
Proprietary |
Property ID |
Data Type |
Writable |
Range |
---|---|---|---|---|---|---|---|
PRESENT_VALUE |
X |
85 |
X 1 |
||||
OUT_OF_SERVICE |
X |
81 |
X |
||||
MAX_PRES_VALUE |
X |
65 |
X |
0–4,294,967,295 |
|||
OBJECT_NAME |
X |
77 |
|||||
SCALE |
X |
187 |
|||||
UNITS |
X |
117 |
X |
0-65,535 |
|||
OBJECT_NAME |
X |
77 |
|||||
SCALE |
X |
187 |
|||||
UNITS |
X |
117 |
X |
0–65,535 |
|||
DESCRIPTION |
X |
28 |
X |
40 characters max |
|||
DEVICE_TYPE |
X |
31 |
X |
20 characters max |
|||
VALUE_SET |
X |
191 |
X |
0–4,294,967,295 |
|||
RELIABILITY |
X |
103 |
X1 |
||||
VALUE_BEFORE_CHANGE |
X |
190 |
|||||
VALUE_CHANGE_TIME |
X |
192 |
|||||
PRESCALE |
X |
185 |
X |
1–65,535 (each part) |
|||
TIME_DELAY |
X 2 |
113 |
X |
0–65,535 |
|||
LIMIT_ENABLE |
X2 |
52 |
X |
||||
EVENT_ENABLE |
X2 |
35 |
X |
||||
ACKED_TRANSITIONS |
X2 |
0 |
|||||
NOTIFY_TYPE |
X2 |
72 |
X |
||||
EVENT_TIME_STAMPS |
X2 |
130 |
|||||
EVENT_MESSAGE_TEXTS |
X2 |
351 | |||||
EVENT_MESSAGE_TEXTS_CONFIG |
X2 |
352 | X | ||||
EVENT_DETECTION_ENABLE |
X2 |
353 | |||||
LIMIT_MONITORING_INTERVAL |
X2 |
182 |
X |
60–604,800 |
|||
HIGH_LIMIT |
X2 |
45 |
X |
0–4,294,967,295 |
|||
LOW_LIMIT |
X2 |
59 |
X |
0–4,294,967,295 |
|||
PULSE_RATE |
X |
186 |
X1 |
||||
NOTIFICATION_CLASS |
X2 |
17 |
X |
1–4,194,302 |
|||
ITEM_REFERENCE |
X |
32527 |
Character String |
||||
STATUS |
X |
512 |
Enumerated |
||||
ENABLED |
X |
673 |
Boolean |
X |
|||
EXECUTION_PRIORITY |
X |
2197 |
Enumerated |
X |
0–3 |
||
OBJECT_CATEGORY |
X |
908 |
Enumerated |
X |
0–249 |
||
ALARM_STATE |
X |
1006 |
Enumerated |
||||
INSTANCE_NUMBER |
X |
32589 |
Unsigned |
||||
OFFLINE |
X |
913 |
Boolean |
||||
PERIODIC_UPDATE |
X |
2192 |
Unsigned |
X |
1–10,000 value |
||
DEBOUNCE |
X |
610 |
Unsigned |
X |
0-65,535ms |
||
SAB_MAC_ADDR |
X |
3645 |
Unsigned |
||||
SLOT |
X |
519 |
Unsigned |
||||
GRAPHIC |
X2 |
32581 |
Character String |
X |
|||
GRAPHIC_ALIAS |
X2 |
32623 |
Character String |
X |
|||
ALARM_MESSAGE_TEXT |
X2 |
536 |
Character String |
X |
255 characters |
||
USER_NAME |
X |
2390 |
Character String |