Network Security Options - BCPro - LIT-12012994 - CH-PCA3613-0 - CH-PCA2513-0 - Field Device - CH-PCA36 Advanced Application Programmable Controller - CH-PCA25 Advanced Application Programmable Controller

Advanced Application Programmable Controllers Protocol Implementation Conformance Statement

Product
Controls > Programmable Controls > CH-PCA36 Advanced Application Programmable Controller
Controls > Programmable Controls > CH-PCA25 Advanced Application Programmable Controller
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12012994
Revision date
2019-11-19

Non-secure Device - is capable of operating without BACnet Network Security

Secure Device - is capable of using BACnet Network Security (NS-SD BIBB)

 

Multiple Application-Specific Keys:

 

Supports encryption (NS-ED BIBB)

 

Key Server (NS-KS BIBB)