Simplex - FireClass - Zettler - Autocall - Configuring and accessing SafeLINC for the European Union and North America - Panel - SAFELINC-CLOUD-CSG - SafeLINC Cloud Services

SafeLINC Cloud Connected Services Gateway: Network Configuration for Gateway Communication

Brand
Simplex
FireClass
Zettler
Autocall
Product
SafeLINC Cloud Services
Document Type
Configuration Guide
Document Number
SAFELINC-CLOUD-CSG
ft:lastPublication
2026-08-04T13:12:07.527000
Product code
557.202.131
Document Revision
3
ft:locale
en-US

Use the appropriate information, based on your location and region, to access the SafeLINC Cloud.

Configuring SafeLINC Cloud for the EU

When you configure firewall or network settings to connect devices to an EU region SafeLINC Cloud, ensure that the firewall accommodates outbound connections for all the listed ports. The customer IT group must provide gateway access to the following sites so that they are not blocked:

SafeLINC Web Architect

To avoid errors, copy and paste the URLs from the following list:

https://eu.safelinc.johnsoncontrols.com

https://api-eu.safelinc.johnsoncontrols.com

https://eu-gateway.xaapbuildings.com

Connected Services Gateway

https://global.azure-devices-provisioning.net

https://aihbtsfirestormprod201.azure-devices.net

https://stgpbtsfirestormprod201.blob.core.windows.net

https://aidpsbtsfirestormprod201.azure-devices-provisioning.net

Configuring SafeLINC Cloud for NA

When you configure firewall or network settings to connect devices in a North American SafeLINC Cloud, ensure that the firewall accommodates outbound connections for all the listed ports. The customer IT group must provide gateway access to the following sites so that they are not blocked:

SafeLINC Web Architect

To avoid errors, copy and paste the URLs from the following list:

https://safelinc.johnsoncontrols.com

https://api.safelinc.johnsoncontrols.com

https://gateway.xaapbuildings.com

Connected Services Gateway

https://global.azure-devices-provisioning.net

https://aihbtsfirestormprod001.azure-devices.net

https://stgpbtsfirestormprod001.blob.core.windows.net/stciothub

https://aidpsbtsfirestormprod001.azure-devices-provisioning.net

Port numbers

The current gateway devices and the CSG use protocols that operate over TCP to communicate with the SafeLINC Cloud. The following table lists the outbound ports that must be open for device communication and data transmission with the SafeLINC Cloud in the network.

Ensure that all the ports listed are open in the network to facilitate communication.

Table 1. Port numbers
Protocol Port
AMQP 5671
MQTT 8883
MQTT over WebSockets 443
HTTPS 443