Simplex - Remove the Old Card - Panel - Fire Alarm Control Unit - 18_SAFELINC-CLOUD-CSG-02 - SafeLINC Cloud

4100U, 4100ES Master Controller Replacement Instructions

Brand
Simplex
Product
SafeLINC Cloud
Document Type
Configuration Guide
Document Number
18_SAFELINC-CLOUD-CSG-02
ft:lastPublication
2026-04-07T10:55:07.618000
Document Revision
Rev. 02
ft:locale
en-US
  1. Locate the CPU daughter card mounted to the CPU motherboard (see Figure 1).
  2. Label and disconnect the service port and display port ribbon cables attached to the CPU daughter card.
  3. Pull the CPU daughter card out of its card slot on the CPU motherboard.
    Figure 1. Contents of CPU Bay