Simplex - Install the New Card - Panel - Fire Alarm Control Unit - 18_SAFELINC-CLOUD-CSG-02 - SafeLINC Cloud

4100U, 4100ES Master Controller Replacement Instructions

Brand
Simplex
Product
SafeLINC Cloud
Document Type
Configuration Guide
Document Number
18_SAFELINC-CLOUD-CSG-02
ft:lastPublication
2026-04-07T10:55:07.618000
Document Revision
Rev. 02
ft:locale
en-US
  1. Make sure that the jumper setting on the new CPU daughter card matches that of the card you have just removed.
  2. Remove the Serial Chip from the old card and install it in the new card.
  3. Install the new CPU daughter card in the slot from which the old card was removed.
  4. Reconnect the service port and display port ribbon cables to the new CPU daughter card.
  5. Close the door to the CPU bay.
  6. Reapply system power at the breaker.
  7. Restore battery power to the cabinet by reconnecting the battery cable at the PDM.
  8. Redress and close the main cabinet door.
  9. Download the system job configuration.

    The system is now ready for normal operation.