Autocall - Multi-loop operation features - Autocall Fire Site Administrator - ACAFSA-0016 - Autocall Fire Site Administrator

Autocall Fire Site Administrator

Brand
Autocall
Product
Autocall Fire Site Administrator
Document Type
Datasheet
Document Number
ACAFSA-0016
ft:lastPublication
2026-08-17T09:02:35.582000
Document Revision
2
ft:locale
en-US
Improved survivability
  • Individual network loops operate independently.

  • In the event of the loss of one or more loops, the remaining loops continue to operate.

Loop independence
  • You can add new loops without impact on existing loops.
System expansion
  • You can install each loop as a stand-alone network, so that local node programming can evolve as required.
  • When construction or renovation reaches completion, you can combine loops for coordinated facility protection.
Multi-Loop requirements
  • Each loop requires a dedicated network interface card (NIC).
  • Autocall Fire Site Administrator supports up to seven ES Net network loops.
Figure 1. Example multi-loop interface with an Autocall Fire Site Administrator computer
Callout Description Callout Description
A ES Net network loop 1 C Additional network loop connections. Up to 7 loops for each network.
B ES Net network loop 2 D ES Net network loop 3
Note: For further information regarding multi-loop or multi-topology support, refer to ES Net Network Applications, Communications, Options and Specifications (AC4100-0076).