Autocall - Individual point service access - Autocall Fire Site Administrator - ACAFSA-0016 - Autocall Fire Site Administrator

Autocall Fire Site Administrator

Brand
Autocall
Product
Autocall Fire Site Administrator
Document Type
Datasheet
Document Number
ACAFSA-0016
ft:lastPublication
2026-08-17T09:02:35.582000
Document Revision
2
ft:locale
en-US

You can use the workstation operator's interface for service-level access to network information that is not normally public. To access private point information for the network, use the Set-Host feature and log on to the database of the network and node. With this operation, qualified service personnel with the correct password access can access and control individual point information.