The Autocall
Fire Site Administrator computer has two Ethernet ports. On ES Net networks, the ES
Net NIC connection uses one Ethernet port. You can use the other Ethernet port to
connect to one of the following devices:
- An agency-listed, dedicated, Fire Alarm LAN
- A customer's LAN
Transient suppressor requirements
Each server and client LAN connection requires a A190-6010 transient suppressor. This does not apply to server to client connections in the same room. For details of the suppressor, see Table 7. For more information, refer to Autocall Fire Site Administrator Remote Clients (ACAFSA-0029).