Autocall - Facilities Maps screens - Autocall Fire Site Administrator - ACAFSA-0016 - Autocall Fire Site Administrator

Autocall Fire Site Administrator

Brand
Autocall
Product
Autocall Fire Site Administrator
Document Type
Datasheet
Document Number
ACAFSA-0016
ft:lastPublication
2026-08-17T09:02:35.582000
Document Revision
2
ft:locale
en-US
Figure 1. Autocall Fire Site Administrator Facilities Maps screen example
Site and floor plan details

The Facilities maps screen prominently displays a site map graphic for site plan and floor plan information. You can customize the level of detail to accurately direct operators to the area of interest.

Facilities maps screen controls
  • Float and move the site map graphic to another monitor.
  • Add icons to identify the location and type of the device of interest.
  • Pan and zoom for more detail.
  • Add programmable coverage zones with selectable areas and a set zoom level.
  • Add a fixed area site plan or key plan, with action buttons and a screen locator as in Figure 1.
Custom logo and main screen background
  • You can customize the logo area on the banner, shown with a Autocall logo in Figure 1. The default size is 250 px x 96 px.
  • You can customize the main screen background that displays before you log on with an image file. The default size is 1920 px x 1163 px.
Action messages
In addition to screen text or graphic information, the operator can receive action messages that include emergency response information and directions. You can edit these action messages in the field for local requirements.
Figure 2. Autocall Fire Site Administrator action messages example
Auto-jump to graphics or alarm list

Select whether an activity causes a jump to a list format or to the associated Facilities Maps screen.

Supported graphics formats
  • DWG import formats: AutoCAD 12 (AC1009) to AutoCAD 2025 (AC1032)
  • Export formats: SVGSCN
  • Import drawing files: SVGSCN, DWG, SVG, PNG, BMP, GIF, and JPG