The Autocall Fire Site Administrator computer is the server on a Autocall Fire Site Administrator fire network. A remote client connects to the Autocall Fire Site Administrator server over https. See the following sections for more information.
The Autocall Fire Site Administrator computer
- Autocall Fire Site Administrator server
- Autocall Fire Site Administrator configurator
Remote clients
- A supervised remote client runs Autocall Fire Site Administrator client software on a Windows computer on the same https network as the Autocall Fire Site Administrator computer. If a supervised remote client disconnects, Autocall Fire Site Administrator indicates a trouble.
- An unsupervised remote client is a device that runs any operating system (OS) with an up-to-date Chrome® browser. An unsupervised remote client has view-only Autocall Fire Site Administrator functionality.
Some Autocall Fire Site Administrator features are inaccessible from a remote device. You can use the Autocall Fire Site Administrator configurator to select the options you require. Refer to Autocall Fire Site Administrator Configurator User Guide (A163832WTD).
Remote client connections
The Autocall Fire Site Administrator server supports a maximum of 60 remote clients that are online simultaneously. You can configure remote clients to connect to a backup server in the event of loss of connection to the primary server. This improves network redundancy.
ES Net support for redundancy on ES Net loops
With the latest ES Net card firmware you can use PanelNet class X, redundancy, when a Autocall Fire Site Administrator node is present.
TCP/IP networks
The minimum required connection speed for connecting a Autocall Fire Site Administrator server or remote client to a TCP/IP local area network is 3 Mbps.
Anti-virus software
- CrowdStrike Windows Sensor 7.29.20108.0
- McAfee™ Total Protection version 16.0 R120 and above
- Norton™ 360 Deluxe version 22.24.5.6 and above
Filtering external points on supervised clients
- By provider: Filter points by list, node, or account.
- By device class: Filter points by device class.
- By alarm category: Filter points by alarm category.
To configure filtering, use the TCP/IP interface settings in the Autocall Fire Site Administrator configurator. For details, refer to Autocall Fire Site Administrator Configurator User Guide (A163832WRA).