Autocall - Ethernet connections - Autocall Fire Site Administrator - ACAFSA-0029 - Autocall Fire Site Administrator

Autocall Fire Site Administrator Remote Clients

Brand
Autocall
Product
Autocall Fire Site Administrator
Document Type
Datasheet
Document Number
ACAFSA-0029
ft:lastPublication
2026-08-17T09:02:46.340000
Document Revision
2
ft:locale
en-US
The Autocall Fire Site Administrator computer has two Ethernet ports. On ES Net networks, the ES Net NIC connection uses one Ethernet port. You can use the other Ethernet port to connect to one of the following devices:
  • An agency-listed, dedicated, Fire Alarm LAN
  • A customer's LAN
For more information about fire alarm network Ethernet switches, refer to Fire Alarm Network Annunciators; Fire Alarm Ethernet Switches (AC4190-0018).

Transient suppressor requirements

Each server and client LAN connection requires a A190-6010 transient suppressor. This does not apply to server and client connections in the same room. For details of the suppressor, see Table 7.